Data Fields
UART2CC26X2_Object Struct Reference

UART2CC26X2 Object. More...

#include <UART2CC26X2.h>

Collaboration diagram for UART2CC26X2_Object:
Collaboration graph
[legend]

Data Fields

UART2_BASE_OBJECT UDMACC26XX_Handle udmaHandle
 
volatile tDMAControlTable * rxDmaEntry
 
volatile tDMAControlTable * txDmaEntry
 
PIN_State pinState
 
PIN_Handle hPin
 
Power_NotifyObj postNotify
 

Detailed Description

UART2CC26X2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ udmaHandle

UART2_BASE_OBJECT UDMACC26XX_Handle UART2CC26X2_Object::udmaHandle

§ rxDmaEntry

volatile tDMAControlTable* UART2CC26X2_Object::rxDmaEntry

§ txDmaEntry

volatile tDMAControlTable* UART2CC26X2_Object::txDmaEntry

§ pinState

PIN_State UART2CC26X2_Object::pinState

§ hPin

PIN_Handle UART2CC26X2_Object::hPin

§ postNotify

Power_NotifyObj UART2CC26X2_Object::postNotify

The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale