Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
zstack_AFAddr_t | srcAddr |
uint16_t | groupID |
uint16_t | clusterId |
uint16_t | macDestAddr |
uint8_t | endpoint |
bool | wasBroadcast |
bool | securityUse |
uint8_t | linkQuality |
uint8_t | correlation |
int_least8_t | rssi |
uint32_t | timestamp |
uint8_t | nwkSeqNum |
uint16_t | macSrcAddr |
uint8_t | radius |
uint16_t | n_payload |
uint8_t * | pPayload |
Structure to send an AF Incoming Message Indication.
uint16_t clusterId |
Message's clusterID
uint8_t correlation |
The raw correlation value of the received data frame
uint8_t endpoint |
Destination endpoint
uint16_t groupID |
Message's group ID - 0 if not group message
uint8_t linkQuality |
The link quality of the received data frame
uint16_t macDestAddr |
MAC header destination short address
uint16_t macSrcAddr |
MAC header source short address
uint16_t n_payload |
Length of the message "payload"
uint8_t nwkSeqNum |
Network header frame sequence number
uint8_t* pPayload |
Pointer to the message "payload"
uint8_t radius |
Message's network radius, 0 mean internal
int_least8_t rssi |
The received RF power in units dBm
bool securityUse |
Set if APS security was used
zstack_AFAddr_t srcAddr |
Source Address, if endpoint is 0xFE, it's an interPAN message
uint32_t timestamp |
Receipt timestamp from MAC
bool wasBroadcast |
Set if network destination was a broadcast address