Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
bool | enable |
bool | has_channel |
uint8_t | channel |
bool | has_endpoint |
uint8_t | endpoint |
bool | has_panID |
uint16_t | panID |
Structure to send an AF Inter-PAN Control Request.
uint8_t channel |
InterPan channel
bool enable |
Set to turn on inter-PAN, Clear to switch back to NIB
uint8_t endpoint |
Endpoint controller
bool has_channel |
Rrue if channel is available, false if not
bool has_endpoint |
True if endpoint is available, false if not
bool has_panID |
True if panID is available, false if not
uint16_t panID |
PAN ID