Z-Stack API Reference  4.40.00.15
_zstack_bdbgenerateinstallcodecrcreq_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t installCode [16]
 

Detailed Description

Structure to send a bdb generate Install Code Request.

Field Documentation

§ installCode

uint8_t installCode[16]

Install code from which CRC will be generated


The documentation for this struct was generated from the following file: