Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint8_t | status |
Structure to send a BDB ZED attempt to Recover Network Request.
uint8_t status |
Indicate if the request was process or not. The request will fail if the device has not been commissioned yet