Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
zstack_NwkState | state |
Network State. | |
uint16_t | nwkAddr |
Network address of device. | |
uint32_t | channelList |
Channel List (bit mask) | |
uint16_t | parentNwkAddr |
Parent's network address. | |
uint16_t | panID |
device's PAN ID | |
uint8_t | depth |
Node depth within network. | |
uint8_t | maxRouters |
uint8_t | maxChildren |
uint32_t | allocatedRouterAddresses |
Allocated Router Addresses. | |
uint32_t | allocatedEndDeviceAddresses |
Allocated End Device Addresses. | |
uint8_t | updateID |
Network Update ID. | |
zstack_LongAddr_t | extendedPANID |
64 bit extended PAN ID, use all 0xFF if don't care | |
Structure to send a Device Force Network Settings Request.
uint8_t maxChildren |
Maximum number of children supported in associated device list (routers only)
uint8_t maxRouters |
Maximum number of routers supported in associated device list (routers only)