Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint16_t | dstAddr |
bool | mtoRoute |
bool | mtoNoCache |
bool | multicast |
uint8_t | radius |
Structure to send a Device Network Route Request.
uint16_t dstAddr |
Network address to discover
bool mtoNoCache |
True if the concentrator has limited cache (only set if mtoRoute is set)
bool mtoRoute |
True if you are announcing a concentrator
bool multicast |
True if the route requested is for a multicast address
uint8_t radius |
Radius of the message