Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint8_t | Status |
uint8_t | dGPStubHandle |
gpdID_t | gpdID |
uint8_t | EndPoint |
gp_SecData_t | gp_SecData |
uint8_t | GPDKey [SEC_KEY_LEN] |
Structure to send a GP Security Response.
uint8_t dGPStubHandle |
The handle used between dGP stub and the higher layers, to match the request with the response
uint8_t EndPoint |
The identifier of the GPD endpoint used in combination with the GPD IEEE address if ApplicationID = 0b010. If ApplicationID = 0b000 this parameter is ignored
gp_SecData_t gp_SecData |
Security parameters
uint8_t GPDKey[SEC_KEY_LEN] |
The security key to be used for GPDF security processing
uint8_t Status |
The status code, as returned by the Green Power EndPoint