Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
zstack_LongAddr_t | extendedPANID |
uint8_t | logicalChan |
uint8_t | stackProfile |
uint8_t | version |
uint8_t | beaconOrder |
uint8_t | superFrameOrder |
bool | permitJoin |
Structure for the network information of a single network
uint8_t beaconOrder |
Beacon Order
zstack_LongAddr_t extendedPANID |
64 bit extended PAN ID
uint8_t logicalChan |
Current logical channel
bool permitJoin |
True if Permit Join set
uint8_t stackProfile |
A ZigBee profile identifier
uint8_t superFrameOrder |
Superframe Order
uint8_t version |
ZigBee Protocol version