Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
bool | tcLinkKey |
zstack_LongAddr_t | ieeeAddr |
uint8_t | key [16] |
uint32_t | txFrmCntr |
uint32_t | rxFrmCntr |
Structure to send a Security APS Link Key Get Response.
zstack_LongAddr_t ieeeAddr |
IEEE Address of the Link Key wanted
uint8_t key[16] |
16 bytes of key data
uint32_t rxFrmCntr |
Receive frame counter
bool tcLinkKey |
True if the key information is for a TC Link Key, false if not
uint32_t txFrmCntr |
Transmit frame counter