Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
bool | wildcardProfileID |
bool | ackRequest |
bool | limitConcentrator |
bool | suppressRouteDisc |
bool | apsSecurity |
bool | skipRouting |
Structure for defining the transaction options when sending a data request.
bool ackRequest |
Set to request APS acknowlegement - This is an application level acknowledgement - meaning that the destination device will acknowledge the message. Only used on messages send direct (unicast).
bool apsSecurity |
Set to enable APS security (link key)
bool limitConcentrator |
Set to limit the message to concentrators only
bool skipRouting |
Setting this option will cause the device to skip routing and try to send the message directly (not multihop). End devices will not send the message to its parent first. Good for only direct (unicast) and broadcast messages.
bool suppressRouteDisc |
Set to suppress intermediate route discoveries (only initial node)
bool wildcardProfileID |
Set to request use of Wildcard Profile ID (OxFFFF)