Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint16_t | sourceAddr |
Source address. | |
uint16_t | panID |
PAN ID. | |
uint8_t | logicalChannel |
Logical channel. | |
bool | permitJoining |
Set if joining allowed. | |
bool | routerCapacity |
Set if there is router capacity available. | |
bool | deviceCapacity |
Set if there is device capacity available. | |
uint8_t | protocolVersion |
Protocol version. | |
uint8_t | stackProfile |
Stack profile. | |
uint8_t | lqi |
LQI. | |
uint8_t | depth |
Network depth. | |
uint8_t | updateID |
Update ID. | |
zstack_LongAddr_t | extendedPANID |
64 bit extended PAN ID | |
Structure to send a ZDO Beacon Notify Indication.