Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint16_t | dstAddr |
uint16_t | bindingTarget |
uint8_t | endpoint |
uint16_t | profileID |
uint8_t | n_inputClusters |
uint16_t * | pInputClusters |
uint8_t | n_outputClusters |
uint16_t * | pOutputClusters |
Structure to send a ZDO End Device .
uint16_t bindingTarget |
The address of the target for the binding. This can be either the primary binding cache device or the short address of the local device.
uint16_t dstAddr |
Destination address, should be 0x0000 for coordinator
uint8_t endpoint |
Source device's endpoint
uint8_t n_inputClusters |
Number of input clusters
uint8_t n_outputClusters |
Number of output clusters
uint16_t* pInputClusters |
Pointer to array of input clusters
uint16_t* pOutputClusters |
Pointer to array of output clusters
uint16_t profileID |
ProfileID which is to be matched between two End_Device_Bind_req received at the ZigBee Coordinator within the timeout value pre-configured in the ZigBee Coordinator.