Z-Stack API Reference
4.40.00.15
|
#include <zstack.h>
Data Fields | |
uint16_t | dstAddr |
uint16_t | nwkAddrOfInterest |
uint8_t | n_userDescriptor |
uint8_t * | pUserDescriptor |
Structure to send a ZDO User Decriptor Set Request.
uint16_t dstAddr |
Destination address
uint8_t n_userDescriptor |
Length of of the User Descriptor (16 max)
uint16_t nwkAddrOfInterest |
The network address of the destination device being queried.
uint8_t* pUserDescriptor |
Pointer to the descriptor