TI BLE5-Stack API Documentation  2.02.01.00
Data Fields
GapAdv_params_t Struct Reference

Data Fields

uint16_t eventProps
 GAP_ADV_PARAM_PROPS
 
GapAdv_filterPolicy_t filterPolicy
 GAP_ADV_PARAM_FILTER_POLICY
 
uint8_t peerAddr [B_ADDR_LEN]
 GAP_ADV_PARAM_PEER_ADDRESS
 
GAP_Peer_Addr_Types_t peerAddrType
 GAP_ADV_PARAM_PEER_ADDRESS_TYPE
 
GapAdv_advChannels_t primChanMap
 GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
 
uint32_t primIntMax
 GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
 
uint32_t primIntMin
 GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
 
GapAdv_primaryPHY_t primPhy
 GAP_ADV_PARAM_PRIMARY_PHY
 
GapAdv_secondaryPHY_t secPhy
 GAP_ADV_PARAM_SECONDARY_PHY
 
uint8_t sid
 GAP_ADV_PARAM_SID
 
int8_t txPower
 NOT CURRENTLY IMPLEMENTED.
 

Detailed Description

Per-advertising set parameters

These can be set with GapAdv_setParam See the specific parameter linked to each element for more information.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale