BLE5-Stack 2.02.00 (SDK 4.40) to BLE5-Stack 2.02.01 (SDK 5.10)¶
This section will describe a way to migrate a project from BLE5-Stack 2.02.00 to a BLE5-Stack 2.02.01 project.
The best way to migrate is to open a new project from the new SDK and transfer your changes and application code over to the new example.
Porting Simple Peripheral¶
For this migration guide, Simple Peripheral from BLE5-Stack 2.02.00 will be ported over to BLE5-Stack 2.02.01. The recommended approach is to start with a BLE5-Stack 2.02.01 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.01 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.02.00 into the BLE5-Stack 2.02.01 example project.
In this example, the following files from BLE5-Stack 2.02.00 were moved into Simple Peripheral BLE5-Stack 2.02.01 example:
simple_peripheral.c
simple_peripheral.h
Move any profiles and services that the application is using to the BLE5-Stack 2.02.01 project.
Transfer the SysConfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13x2 / 26x2 SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13x2 / 26x2 SDK.
For additional information on how BLE5-Stack 2.02.01 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.
Porting Simple Central¶
This section of the migration guide will focus on porting Simple Central from BLE5-Stack 2.02.00 to the BLE5-Stack 2.02.01. The recommended approach is to start with a BLE5-Stack 2.02.01 project that contains the same base functionality as theporting target project and merge in any custom functionality.
Choose a BLE5-Stack 2.02.01 example project that contains your target project’s base functionality.
Transfer all modified application files from BLE5-Stack 2.02.00 into the BLE5-Stack 2.02.01 example project.
In this example, the following files from BLE5-Stack 2.02.00 were moved into Simple Central BLE5-Stack 2.02.01 example:
simple_central.c
simple_central.h
Modify
connRec_t
definition insimple_central.c
such that thecharHandle
is of typeuint16_t
as shown below:1 2 3 4 5 6 7 8
// Connected device information typedef struct { uint16_t connHandle; // Connection Handle uint16_t addr[B_ADDR_LEN]; // Peer Device Address uint16_t charHandle; // Characteristic Handle Clock_Struct *pRssiClock; // pointer to clock struct } connRec_t;
Modify
main.c
in the BLE5-Stack 2.02.01 example if additional tasks were added in the BLE5-Stack 2.02.00 project.Move any profiles and services that the application is using to the BLE5-Stack 2.02.01 project.
Transfer the Sysconfig settings either visually through the GUI or open both the old and the new project .syscfg files and copy-paste the desired settings.
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC13x2 / 26x2 SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC13x2 / 26x2 SDK.
For additional information on how BLE5-Stack 2.01.02 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.
A Few Noteworthy Changes from BLE5-Stack 2.02.00 to BLE5-Stack 2.02.01¶
You can follow the guide above without addressing these updates, they are listed for your information only. All fine grained details might not be mentioned, please refer to the specific example you need to port and to a compare between the old and new project files. Please refer to the BLE5-Stack Release Notes for all the details.
- Agama 704 device support has been added to SDK.
- Examples for Agama 704 devices have been added to SDK.
- Agama 704 devices included in SysConfig.