DMM API Reference
3.10.00.15
|
Policy Information dynamically updated. More...
#include <dmm_policy.h>
Public Attributes | |
uint32_t | stackID |
ID to define the stack using current policy. | |
uint8_t | currentWeight |
The current weight value of the policy. | |
uint8_t | defaultPriority |
The default priority of the policy. | |
Policy Information dynamically updated.