52 #ifndef ti_drivers_ecdh_ECDHCC26X1__include 53 #define ti_drivers_ecdh_ECDHCC26X1__include 60 #include <ti/devices/DeviceFamily.h> 61 #include DeviceFamily_constructPath(driverlib/rom_ecc.h) 87 uint32_t eccWorkZone[171];
ECDHCC26X1 Hardware Attributes.
Definition: ECDHCC26X1.h:73
bool isOpen
Definition: ECDHCC26X1.h:83
uint8_t dummy
Definition: ECDHCC26X1.h:74
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X1.h:84
ECDHCC26X1 Object.
Definition: ECDHCC26X1.h:82
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X1.h:85
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:636
ECC_State eccState
Definition: ECDHCC26X1.h:86
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
ECDH_ReturnBehavior
The way in which ECC function calls return after performing an encryption + authentication or decrypt...
Definition: ECDH.h:536