Data Fields
ECDHCC26X1_HWAttrs Struct Reference

ECDHCC26X1 Hardware Attributes. More...

#include <ECDHCC26X1.h>

Data Fields

uint8_t dummy
 

Detailed Description

ECDHCC26X1 Hardware Attributes.

ECC26XX hardware attributes should be included in the board file and pointed to by the ECDH_config struct.

Field Documentation

§ dummy

uint8_t ECDHCC26X1_HWAttrs::dummy

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale