Data Fields
DisplaySharp_Object Struct Reference

#include <DisplaySharp.h>

Collaboration diagram for DisplaySharp_Object:
Collaboration graph
[legend]

Data Fields

Graphics_Context g_sContext
 
SPI_Handle hSpi
 
Display_LineClearMode lineClearMode
 
Graphics_Display g_sDisplay
 
DisplaySharpColor_t displayColor
 
SemaphoreP_Handle semLCD
 
uint8_t * displayBuffer
 

Field Documentation

§ g_sContext

Graphics_Context DisplaySharp_Object::g_sContext

§ hSpi

SPI_Handle DisplaySharp_Object::hSpi

§ lineClearMode

Display_LineClearMode DisplaySharp_Object::lineClearMode

§ g_sDisplay

Graphics_Display DisplaySharp_Object::g_sDisplay

§ displayColor

DisplaySharpColor_t DisplaySharp_Object::displayColor

§ semLCD

SemaphoreP_Handle DisplaySharp_Object::semLCD

§ displayBuffer

uint8_t* DisplaySharp_Object::displayBuffer

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale