Data Fields
ECDSACC26X2_Object Struct Reference

ECDSACC26X2 Object. More...

#include <ECDSACC26X2.h>

Collaboration diagram for ECDSACC26X2_Object:
Collaboration graph
[legend]

Data Fields

TRNG_Config trngConfig
 
TRNGCC26XX_Object trngObject
 
TRNGCC26XX_HWAttrs trngHwAttrs
 
TRNG_Handle trngHandle
 
bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t operationStatus
 
ECDSA_Operation operation
 
ECDSA_OperationType operationType
 
ECDSA_CallbackFxn callbackFxn
 
ECDSACC26X2_stateMachineFxn fsmFxn
 
ECDSA_ReturnBehavior returnBehavior
 
ECDSACC26X2_FsmState fsmState
 
uint32_t semaphoreTimeout
 
uint32_t resultAddress
 
uint32_t * scratchNumber1
 
uint32_t * scratchNumber2
 
CryptoKey pmsnKey
 

Detailed Description

ECDSACC26X2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ trngConfig

TRNG_Config ECDSACC26X2_Object::trngConfig

§ trngObject

TRNGCC26XX_Object ECDSACC26X2_Object::trngObject

§ trngHwAttrs

TRNGCC26XX_HWAttrs ECDSACC26X2_Object::trngHwAttrs

§ trngHandle

TRNG_Handle ECDSACC26X2_Object::trngHandle

§ isOpen

bool ECDSACC26X2_Object::isOpen

§ operationInProgress

bool ECDSACC26X2_Object::operationInProgress

§ operationCanceled

bool ECDSACC26X2_Object::operationCanceled

§ operationStatus

int_fast16_t ECDSACC26X2_Object::operationStatus

§ operation

ECDSA_Operation ECDSACC26X2_Object::operation

§ operationType

ECDSA_OperationType ECDSACC26X2_Object::operationType

§ callbackFxn

ECDSA_CallbackFxn ECDSACC26X2_Object::callbackFxn

§ fsmFxn

ECDSACC26X2_stateMachineFxn ECDSACC26X2_Object::fsmFxn

§ returnBehavior

ECDSA_ReturnBehavior ECDSACC26X2_Object::returnBehavior

§ fsmState

ECDSACC26X2_FsmState ECDSACC26X2_Object::fsmState

§ semaphoreTimeout

uint32_t ECDSACC26X2_Object::semaphoreTimeout

§ resultAddress

uint32_t ECDSACC26X2_Object::resultAddress

§ scratchNumber1

uint32_t* ECDSACC26X2_Object::scratchNumber1

§ scratchNumber2

uint32_t* ECDSACC26X2_Object::scratchNumber2

§ pmsnKey

CryptoKey ECDSACC26X2_Object::pmsnKey

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale