Data Fields
UDMACC26XX_HWAttrs Struct Reference

UDMACC26XX hardware attributes. More...

#include <UDMACC26XX.h>

Data Fields

uint32_t baseAddr
 
PowerCC26XX_Resource powerMngrId
 
uint8_t intNum
 
uint8_t intPriority
 UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create(). More...
 

Detailed Description

UDMACC26XX hardware attributes.

Field Documentation

§ baseAddr

uint32_t UDMACC26XX_HWAttrs::baseAddr

§ powerMngrId

PowerCC26XX_Resource UDMACC26XX_HWAttrs::powerMngrId

UDMACC26XX Peripheral's power manager ID

§ intNum

uint8_t UDMACC26XX_HWAttrs::intNum

UDMACC26XX error interrupt number

§ intPriority

uint8_t UDMACC26XX_HWAttrs::intPriority

UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).

(7 << 5) will apply the lowest priority.

(1 << 5) will apply the highest priority.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale