DMM API Reference
3.20.00.07
|
Dual Mode Manager RF API remapping.
The dmm_rfmap header file remaps select functions in the RF driver API the DMM equivalents that are defined in the dmm_schedular module so that priorities and timing can be set according to the dual mode manager policy
Go to the source code of this file.
Macros | |
#define | RF_open DMMSch_rfOpen |
#define | RF_postCmd DMMSch_rfPostCmd |
#define | RF_runCmd DMMSch_rfRunCmd |
#define | RF_scheduleCmd DMMSch_rfScheduleCmd |
#define | RF_runScheduleCmd DMMSch_rfRunScheduleCmd |
#define | RF_cancelCmd DMMSch_rfCancelCmd |
#define | RF_flushCmd DMMSch_rfFlushCmd |
#define | RF_runImmediateCmd DMMSch_rfRunImmediateCmd |
#define | RF_runDirectCmd DMMSch_rfRunDirectCmd |
#define | RF_requestAccess DMMSch_rfRequestAccess |