DMM API Reference
3.20.00.07
|
Structure used to define a DMM Policy. More...
#include <dmm_policy.h>
Public Attributes | |
uint32_t | state |
application state of a policy | |
uint8_t | weight |
amount of adjusted priority for stack activities specified in .appliedActivity | |
uint16_t | timingConstraint |
reserved for future usage | |
uint32_t | appliedActivity |
uint16_t | pause |
whether or not the specified stack's application is paused during the state:0 not paused, 0x0001 paused | |
Structure used to define a DMM Policy.
uint32_t DMMPolicy_State::appliedActivity |
Specified the activities of which priority is/are adjusted by .weight final Priority = GPT (Stack level priority) + weight (Application Level)