ADCCC26XX Object. More...
#include <ADCCC26XX.h>
Data Fields | |
PIN_State | pinState |
PIN_Handle | pinHandle |
bool | isOpen |
bool | isProtected |
ADCCC26XX Object.
The application must not access any member variables of this structure!
PIN_State ADCCC26XX_Object::pinState |
< Pin state object Pin handle
PIN_Handle ADCCC26XX_Object::pinHandle |
Flag if the instance is in use
bool ADCCC26XX_Object::isOpen |
Flag to indicate if thread safety is ensured by the driver
bool ADCCC26XX_Object::isProtected |