rflib
|
Bluetooth 5 Radio Setup Command for all PHYs. More...
#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x1820. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t mainMode:2 | |
PHY to use for non-BLE commands: 0: 1 Mbps 1: 2 Mbps 2: Coded 3: Reserved More... | |
uint8_t coding:1 | |
Coding to use for TX if coded PHY is selected for non-BLE commands 0: S = 8 (125 kbps) 1: S = 2 (500 kbps) More... | |
} | defaultPhy |
uint8_t | loDivider |
LO divider setting to use. Supported values: 0 or 2. More... | |
struct { | |
uint16_t frontEndMode:3 | |
0x00: Differential mode 0x01: Single-ended mode RFP 0x02: Single-ended mode RFN 0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX) 0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX) Others: Reserved More... | |
uint16_t biasMode:1 | |
0: Internal bias 1: External bias More... | |
uint16_t analogCfgMode:6 | |
0x00: Write analog configuration. Required first time after boot and when changing frequency band or front-end configuration 0x2D: Keep analog configuration. May be used after standby or when changing mode with the same frequency band and front-end configuration Others: Reserved More... | |
uint16_t bNoFsPowerUp:1 | |
0: Power up frequency synth 1: Do not power up frequency synth More... | |
uint16_t __pad0__:1 | |
uint16_t bSynthNarrowBand:1 | |
0: Normal synth mode 1: Narrow-band synth mode More... | |
} | config |
Configuration options. More... | |
uint16_t | txPower |
Default transmit power. More... | |
uint32_t * | pRegOverrideCommon |
Pointer to a list of hardware and configuration registers to override during common initialization. If NULL, no override is used. More... | |
uint32_t * | pRegOverride1Mbps |
Pointer to a list of hardware and configuration registers to override when selecting 1 Mbps PHY mode. If NULL, no override is used. More... | |
uint32_t * | pRegOverride2Mbps |
Pointer to a list of hardware and configuration registers to override when selecting 2 Mbps PHY mode. If NULL, no override is used. More... | |
uint32_t * | pRegOverrideCoded |
Pointer to a list of hardware and configuration registers to override when selecting coded PHY mode. If NULL, no override is used. More... | |
Bluetooth 5 Radio Setup Command for all PHYs.
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::commandNo |
The command ID number 0x1820.
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t* rfc_CMD_BLE5_RADIO_SETUP_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_BLE5_RADIO_SETUP_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_BLE5_RADIO_SETUP_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_BLE5_RADIO_SETUP_s::condition |
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::mainMode |
PHY to use for non-BLE commands:
0: 1 Mbps
1: 2 Mbps
2: Coded
3: Reserved
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::coding |
Coding to use for TX if coded PHY is selected for non-BLE commands
0: S = 8 (125 kbps)
1: S = 2 (500 kbps)
struct { ... } rfc_CMD_BLE5_RADIO_SETUP_s::defaultPhy |
uint8_t rfc_CMD_BLE5_RADIO_SETUP_s::loDivider |
LO divider setting to use. Supported values: 0 or 2.
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::frontEndMode |
0x00: Differential mode
0x01: Single-ended mode RFP
0x02: Single-ended mode RFN
0x05 Single-ended mode RFP with external frontend control on RF pins (RFN and RXTX)
0x06 Single-ended mode RFN with external frontend control on RF pins (RFP and RXTX)
Others: Reserved
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::biasMode |
0: Internal bias
1: External bias
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::analogCfgMode |
0x00: Write analog configuration.
Required first time after boot and when changing frequency band or front-end configuration
0x2D: Keep analog configuration.
May be used after standby or when changing mode with the same frequency band and front-end configuration
Others: Reserved
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::bNoFsPowerUp |
0: Power up frequency synth
1: Do not power up frequency synth
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::__pad0__ |
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::bSynthNarrowBand |
0: Normal synth mode
1: Narrow-band synth mode
struct { ... } rfc_CMD_BLE5_RADIO_SETUP_s::config |
Configuration options.
uint16_t rfc_CMD_BLE5_RADIO_SETUP_s::txPower |
Default transmit power.
uint32_t* rfc_CMD_BLE5_RADIO_SETUP_s::pRegOverrideCommon |
Pointer to a list of hardware and configuration registers to override during common initialization. If NULL, no override is used.
uint32_t* rfc_CMD_BLE5_RADIO_SETUP_s::pRegOverride1Mbps |
Pointer to a list of hardware and configuration registers to override when selecting 1 Mbps PHY mode. If NULL, no override is used.
uint32_t* rfc_CMD_BLE5_RADIO_SETUP_s::pRegOverride2Mbps |
Pointer to a list of hardware and configuration registers to override when selecting 2 Mbps PHY mode. If NULL, no override is used.
uint32_t* rfc_CMD_BLE5_RADIO_SETUP_s::pRegOverrideCoded |
Pointer to a list of hardware and configuration registers to override when selecting coded PHY mode. If NULL, no override is used.