rflib
Data Fields
rfc_CMD_FS_s Struct Reference

Frequency Synthesizer Programming Command. More...

#include <rf_common_cmd.h>

Collaboration diagram for rfc_CMD_FS_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x0803. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
uint16_t frequency
 The frequency in MHz to tune to. More...
 
uint16_t fractFreq
 Fractional part of the frequency to tune to. More...
 
struct {
   uint8_t   bTxMode:1
 0: Start synth in RX mode
1: Start synth in TX mode More...
 
   uint8_t   refFreq:6
 0: Use default reference frequency
Others: Use reference frequency 48 MHz/refFreq More...
 
synthConf
 
uint8_t __dummy0
 Reserved, always write 0 More...
 
uint8_t __dummy1
 Reserved More...
 
uint8_t __dummy2
 Reserved More...
 
uint16_t __dummy3
 Reserved More...
 

Detailed Description

Frequency Synthesizer Programming Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_FS_s::commandNo

The command ID number 0x0803.

§ status

uint16_t rfc_CMD_FS_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t* rfc_CMD_FS_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_FS_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_FS_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_FS_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_FS_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_FS_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger

struct { ... } rfc_CMD_FS_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_FS_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_FS_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition

struct { ... } rfc_CMD_FS_s::condition

§ frequency

uint16_t rfc_CMD_FS_s::frequency

The frequency in MHz to tune to.

§ fractFreq

uint16_t rfc_CMD_FS_s::fractFreq

Fractional part of the frequency to tune to.

§ bTxMode

uint8_t rfc_CMD_FS_s::bTxMode

0: Start synth in RX mode
1: Start synth in TX mode

§ refFreq

uint8_t rfc_CMD_FS_s::refFreq

0: Use default reference frequency
Others: Use reference frequency 48 MHz/refFreq

§ synthConf

struct { ... } rfc_CMD_FS_s::synthConf

§ __dummy0

uint8_t rfc_CMD_FS_s::__dummy0

Reserved, always write 0

§ __dummy1

uint8_t rfc_CMD_FS_s::__dummy1

Reserved

§ __dummy2

uint8_t rfc_CMD_FS_s::__dummy2

Reserved

§ __dummy3

uint16_t rfc_CMD_FS_s::__dummy3

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale