rflib
Data Fields
rfc_CMD_READ_RFREG_s Struct Reference

Read RF Core Hardware Register. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0601. More...
 
uint16_t address
 The offset from the start of the RF core HW register bank (0x40040000) More...
 
uint32_t value
 Returned value of the register. More...
 

Detailed Description

Read RF Core Hardware Register.

Field Documentation

§ commandNo

uint16_t rfc_CMD_READ_RFREG_s::commandNo

The command ID number 0x0601.

§ address

uint16_t rfc_CMD_READ_RFREG_s::address

The offset from the start of the RF core HW register bank (0x40040000)

§ value

uint32_t rfc_CMD_READ_RFREG_s::value

Returned value of the register.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale