rflib
Data Fields
rfc_CMD_SET_RAT_CMP_s Struct Reference

Set Radio Timer Channel in Compare Mode. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x000A. More...
 
uint8_t ratCh
 The radio timer channel number. More...
 
uint8_t __dummy0
 
ratmr_t compareTime
 The time at which the compare occurs. More...
 

Detailed Description

Set Radio Timer Channel in Compare Mode.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_RAT_CMP_s::commandNo

The command ID number 0x000A.

§ ratCh

uint8_t rfc_CMD_SET_RAT_CMP_s::ratCh

The radio timer channel number.

§ __dummy0

uint8_t rfc_CMD_SET_RAT_CMP_s::__dummy0

§ compareTime

ratmr_t rfc_CMD_SET_RAT_CMP_s::compareTime

The time at which the compare occurs.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale