rflib
Data Fields
rfc_CMD_START_RAT_s Struct Reference

Asynchronously Start Radio Timer Command. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0405. More...
 

Detailed Description

Asynchronously Start Radio Timer Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_START_RAT_s::commandNo

The command ID number 0x0405.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale