rflib
Data Fields
rfc_CMD_TX_TEST_s Struct Reference

Transmitter Test Command. More...

#include <rf_common_cmd.h>

Collaboration diagram for rfc_CMD_TX_TEST_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x0808. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bUseCw:1
 0: Send modulated signal
1: Send continuous wave More...
 
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   whitenMode:2
 0: No whitening
1: Default whitening
2: PRBS-15
3: PRBS-32 More...
 
config
 
uint8_t __dummy0
 
uint16_t txWord
 Value to send to the modem before whitening. More...
 
uint8_t __dummy1
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
uint32_t syncWord
 Sync word to use for transmitter. More...
 
ratmr_t endTime
 Time to end the operation. More...
 

Detailed Description

Transmitter Test Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_TX_TEST_s::commandNo

The command ID number 0x0808.

§ status

uint16_t rfc_CMD_TX_TEST_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t* rfc_CMD_TX_TEST_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_TX_TEST_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_TX_TEST_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_TX_TEST_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_TX_TEST_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_TX_TEST_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger

struct { ... } rfc_CMD_TX_TEST_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_TX_TEST_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_TX_TEST_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition

struct { ... } rfc_CMD_TX_TEST_s::condition

§ bUseCw

uint8_t rfc_CMD_TX_TEST_s::bUseCw

0: Send modulated signal
1: Send continuous wave

§ bFsOff

uint8_t rfc_CMD_TX_TEST_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

§ whitenMode

uint8_t rfc_CMD_TX_TEST_s::whitenMode

0: No whitening
1: Default whitening
2: PRBS-15
3: PRBS-32

§ config

struct { ... } rfc_CMD_TX_TEST_s::config

§ __dummy0

uint8_t rfc_CMD_TX_TEST_s::__dummy0

§ txWord

uint16_t rfc_CMD_TX_TEST_s::txWord

Value to send to the modem before whitening.

§ __dummy1

uint8_t rfc_CMD_TX_TEST_s::__dummy1

§ endTrigger

struct { ... } rfc_CMD_TX_TEST_s::endTrigger

Trigger classifier for ending the operation.

§ syncWord

uint32_t rfc_CMD_TX_TEST_s::syncWord

Sync word to use for transmitter.

§ endTime

ratmr_t rfc_CMD_TX_TEST_s::endTime

Time to end the operation.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale