rflib
Data Fields
rfc_CMD_UPDATE_HPOSC_FREQ_s Struct Reference

Set New Frequency Offset for HPOSC. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0608. More...
 
int16_t freqOffset
 Relative frequency offset, signed, scaled by 2-22 More...
 

Detailed Description

Set New Frequency Offset for HPOSC.

Field Documentation

§ commandNo

uint16_t rfc_CMD_UPDATE_HPOSC_FREQ_s::commandNo

The command ID number 0x0608.

§ freqOffset

int16_t rfc_CMD_UPDATE_HPOSC_FREQ_s::freqOffset

Relative frequency offset, signed, scaled by 2-22


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale