rflib
|
#include <rf_ble_cmd.h>
Data Fields | |
struct { | |
uint16_t advDataId:12 | |
If bValid = 1: Last Advertising Data ID (DID) for the Advertising Set ID (SID) corresponding to the entry number in the array. More... | |
uint16_t mode:2 | |
0: Entry is invalid (always receive packet with the given SID) 1: Entry is valid (ignore packets with the given SID where DID equals advDataId )2: Entry is blocked (always ignore packet with the given SID) 3: Reserved More... | |
} | advDataInfo |
uint16_t rfc_ble5AdiEntry_s::advDataId |
If bValid
= 1: Last Advertising Data ID (DID) for the Advertising Set ID (SID) corresponding to the entry number in the array.
uint16_t rfc_ble5AdiEntry_s::mode |
0: Entry is invalid (always receive packet with the given SID)
1: Entry is valid (ignore packets with the given SID where DID equals advDataId
)
2: Entry is blocked (always ignore packet with the given SID)
3: Reserved
struct { ... } rfc_ble5AdiEntry_s::advDataInfo |