#include <rf_ble_cmd.h>
|
struct { |
uint8_t __pad0__:2 |
|
uint8_t deviceAddrType:1 |
| The type of the device address – public (0) or random (1) More...
|
|
} | advConfig |
|
uint8_t | __dummy0 |
|
uint8_t | __dummy1 |
|
uint8_t | auxPtrTargetType |
| Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed. More...
|
|
ratmr_t | auxPtrTargetTime |
| Time of start of packet to which auxPtr points. More...
|
|
uint8_t * | pAdvPkt |
| Pointer to extended advertising packet for the ADV_EXT_IND packet. More...
|
|
uint16_t * | pDeviceAddress |
| Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType is inverted. More...
|
|
§ __pad0__
uint8_t rfc_ble5AdvExtPar_s::__pad0__ |
§ deviceAddrType
uint8_t rfc_ble5AdvExtPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
§ advConfig
struct { ... } rfc_ble5AdvExtPar_s::advConfig |
§ __dummy0
uint8_t rfc_ble5AdvExtPar_s::__dummy0 |
§ __dummy1
uint8_t rfc_ble5AdvExtPar_s::__dummy1 |
§ auxPtrTargetType
uint8_t rfc_ble5AdvExtPar_s::auxPtrTargetType |
Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed.
§ auxPtrTargetTime
ratmr_t rfc_ble5AdvExtPar_s::auxPtrTargetTime |
Time of start of packet to which auxPtr points.
§ pAdvPkt
uint8_t* rfc_ble5AdvExtPar_s::pAdvPkt |
Pointer to extended advertising packet for the ADV_EXT_IND packet.
§ pDeviceAddress
uint16_t* rfc_ble5AdvExtPar_s::pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType
is inverted.
The documentation for this struct was generated from the following file: