rflib
Data Fields
rfc_bleInitiatorPar_s Struct Reference

#include <rf_ble_cmd.h>

Collaboration diagram for rfc_bleInitiatorPar_s:
Collaboration graph
[legend]

Data Fields

dataQueue_tpRxQ
 Pointer to receive queue. More...
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically remove ignored packets from Rx queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically remove packets with CRC error from Rx queue. More...
 
   uint8_t   bAutoFlushEmpty:1
 If 1, automatically remove empty packets from Rx queue. More...
 
   uint8_t   bIncludeLenByte:1
 If 1, include the received length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the Rx queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status word to the packet in the Rx queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the Rx queue. More...
 
rxConfig
 Configuration bits for the receive queue entries. More...
 
struct {
   uint8_t   bUseWhiteList:1
 Initiator filter policy
0: Use specific peer address
1: Use white list. More...
 
   uint8_t   bDynamicWinOffset:1
 0: No dynamic WinOffset insertion
1: Use dynamic WinOffset insertion More...
 
   uint8_t   deviceAddrType:1
 The type of the device address – public (0) or random (1) More...
 
   uint8_t   peerAddrType:1
 The type of the peer address – public (0) or random (1) More...
 
   uint8_t   bStrictLenFilter:1
 0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type More...
 
   uint8_t   chSel:1
 0: Do not report support of Channel Selection Algorithm #2
1: Report support of Channel Selection Algorithm #2 More...
 
initConfig
 
uint8_t __dummy0
 
uint8_t connectReqLen
 Size of connect request data. More...
 
uint8_t * pConnectReqData
 Pointer to buffer containing LLData to go in the CONNECT_IND (CONNECT_REQ) More...
 
uint16_t * pDeviceAddress
 Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by initConfig.deviceAddrType is inverted. More...
 
rfc_bleWhiteListEntry_tpWhiteList
 Pointer (with least significant bit set to 0) to white list or peer address. If least significant bit is 1, the address type given by initConfig.peerAddrType is inverted. More...
 
ratmr_t connectTime
 Indication of timer value of the first possible start time of the first connection event. Set to the calculated value if a connection is made and to the next possible connection time if not. More...
 
uint16_t __dummy1
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
timeoutTrigger
 Trigger that causes the device to stop receiving as soon as allowed. More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger that causes the device to stop receiving as soon as allowed. More...
 
ratmr_t timeoutTime
 Time used together with timeoutTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT. More...
 
ratmr_t endTime
 Time used together with endTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED. More...
 

Field Documentation

§ pRxQ

dataQueue_t* rfc_bleInitiatorPar_s::pRxQ

Pointer to receive queue.

§ bAutoFlushIgnored

uint8_t rfc_bleInitiatorPar_s::bAutoFlushIgnored

If 1, automatically remove ignored packets from Rx queue.

§ bAutoFlushCrcErr

uint8_t rfc_bleInitiatorPar_s::bAutoFlushCrcErr

If 1, automatically remove packets with CRC error from Rx queue.

§ bAutoFlushEmpty

uint8_t rfc_bleInitiatorPar_s::bAutoFlushEmpty

If 1, automatically remove empty packets from Rx queue.

§ bIncludeLenByte

uint8_t rfc_bleInitiatorPar_s::bIncludeLenByte

If 1, include the received length byte in the stored packet; otherwise discard it.

§ bIncludeCrc

uint8_t rfc_bleInitiatorPar_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

§ bAppendRssi

uint8_t rfc_bleInitiatorPar_s::bAppendRssi

If 1, append an RSSI byte to the packet in the Rx queue.

§ bAppendStatus

uint8_t rfc_bleInitiatorPar_s::bAppendStatus

If 1, append a status word to the packet in the Rx queue.

§ bAppendTimestamp

uint8_t rfc_bleInitiatorPar_s::bAppendTimestamp

If 1, append a timestamp to the packet in the Rx queue.

§ rxConfig

struct { ... } rfc_bleInitiatorPar_s::rxConfig

Configuration bits for the receive queue entries.

§ bUseWhiteList

uint8_t rfc_bleInitiatorPar_s::bUseWhiteList

Initiator filter policy
0: Use specific peer address
1: Use white list.

§ bDynamicWinOffset

uint8_t rfc_bleInitiatorPar_s::bDynamicWinOffset

0: No dynamic WinOffset insertion
1: Use dynamic WinOffset insertion

§ deviceAddrType

uint8_t rfc_bleInitiatorPar_s::deviceAddrType

The type of the device address – public (0) or random (1)

§ peerAddrType

uint8_t rfc_bleInitiatorPar_s::peerAddrType

The type of the peer address – public (0) or random (1)

§ bStrictLenFilter

uint8_t rfc_bleInitiatorPar_s::bStrictLenFilter

0: Accept any packet with a valid advertising packet length
1: Discard messages with illegal length for the given packet type

§ chSel

uint8_t rfc_bleInitiatorPar_s::chSel

0: Do not report support of Channel Selection Algorithm #2
1: Report support of Channel Selection Algorithm #2

§ initConfig

struct { ... } rfc_bleInitiatorPar_s::initConfig

§ __dummy0

uint8_t rfc_bleInitiatorPar_s::__dummy0

§ connectReqLen

uint8_t rfc_bleInitiatorPar_s::connectReqLen

Size of connect request data.

§ pConnectReqData

uint8_t* rfc_bleInitiatorPar_s::pConnectReqData

Pointer to buffer containing LLData to go in the CONNECT_IND (CONNECT_REQ)

§ pDeviceAddress

uint16_t* rfc_bleInitiatorPar_s::pDeviceAddress

Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by initConfig.deviceAddrType is inverted.

§ pWhiteList

rfc_bleWhiteListEntry_t* rfc_bleInitiatorPar_s::pWhiteList

Pointer (with least significant bit set to 0) to white list or peer address. If least significant bit is 1, the address type given by initConfig.peerAddrType is inverted.

§ connectTime

ratmr_t rfc_bleInitiatorPar_s::connectTime

Indication of timer value of the first possible start time of the first connection event. Set to the calculated value if a connection is made and to the next possible connection time if not.

§ __dummy1

uint16_t rfc_bleInitiatorPar_s::__dummy1

§ triggerType

uint8_t rfc_bleInitiatorPar_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_bleInitiatorPar_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_bleInitiatorPar_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_bleInitiatorPar_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ timeoutTrigger

struct { ... } rfc_bleInitiatorPar_s::timeoutTrigger

Trigger that causes the device to stop receiving as soon as allowed.

§ endTrigger

struct { ... } rfc_bleInitiatorPar_s::endTrigger

Trigger that causes the device to stop receiving as soon as allowed.

§ timeoutTime

ratmr_t rfc_bleInitiatorPar_s::timeoutTime

Time used together with timeoutTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_RXTIMEOUT.

§ endTime

ratmr_t rfc_bleInitiatorPar_s::endTime

Time used together with endTrigger that causes the device to stop receiving as soon as allowed, ending with BLE_DONE_ENDED.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale