#include <rf_ble_cmd.h>
|
uint8_t | size |
| Number of while list entries. Used in the first entry of the list only. More...
|
|
struct { |
uint8_t bEnable:1 |
| 1 if the entry is in use, 0 if the entry is not in use More...
|
|
uint8_t addrType:1 |
| The type address in the entry – public (0) or random (1) More...
|
|
uint8_t bWlIgn:1 |
| 1 if the entry is to be ignored by a scanner if the AdvDataInfo field is not present, 0 otherwise. Used to mask out entries that have already been scanned and reported. More...
|
|
uint8_t __pad0__:1 |
|
uint8_t bPrivIgn:1 |
| 1 if the entry is to be ignored as part of a privacy algorithm, 0 otherwise More...
|
|
} | conf |
|
uint16_t | address |
| Least significant 16 bits of the address contained in the entry. More...
|
|
uint32_t | addressHi |
| Most significant 32 bits of the address contained in the entry. More...
|
|
§ size
uint8_t rfc_bleWhiteListEntry_s::size |
Number of while list entries. Used in the first entry of the list only.
§ bEnable
uint8_t rfc_bleWhiteListEntry_s::bEnable |
1 if the entry is in use, 0 if the entry is not in use
§ addrType
uint8_t rfc_bleWhiteListEntry_s::addrType |
The type address in the entry – public (0) or random (1)
§ bWlIgn
uint8_t rfc_bleWhiteListEntry_s::bWlIgn |
1 if the entry is to be ignored by a scanner if the AdvDataInfo field is not present, 0 otherwise. Used to mask out entries that have already been scanned and reported.
§ __pad0__
uint8_t rfc_bleWhiteListEntry_s::__pad0__ |
§ bPrivIgn
uint8_t rfc_bleWhiteListEntry_s::bPrivIgn |
1 if the entry is to be ignored as part of a privacy algorithm, 0 otherwise
§ conf
struct { ... } rfc_bleWhiteListEntry_s::conf |
§ address
uint16_t rfc_bleWhiteListEntry_s::address |
Least significant 16 bits of the address contained in the entry.
§ addressHi
uint32_t rfc_bleWhiteListEntry_s::addressHi |
Most significant 32 bits of the address contained in the entry.
The documentation for this struct was generated from the following file: