rflib
Data Fields
rfc_ieeeRxOutput_s Struct Reference

#include <rf_ieee_cmd.h>

Data Fields

uint8_t nTxAck
 Total number of transmitted ACK frames. More...
 
uint8_t nRxBeacon
 Number of received beacon frames. More...
 
uint8_t nRxData
 Number of received data frames. More...
 
uint8_t nRxAck
 Number of received acknowledgement frames. More...
 
uint8_t nRxMacCmd
 Number of received MAC command frames. More...
 
uint8_t nRxReserved
 Number of received frames with reserved frame type. More...
 
uint8_t nRxNok
 Number of received frames with CRC error. More...
 
uint8_t nRxIgnored
 Number of frames received that are to be ignored. More...
 
uint8_t nRxBufFull
 Number of received frames discarded because the Rx buffer was full. More...
 
int8_t lastRssi
 RSSI of last received frame. More...
 
int8_t maxRssi
 Highest RSSI observed in the operation. More...
 
uint8_t __dummy0
 
ratmr_t beaconTimeStamp
 Time stamp of last received beacon frame. More...
 

Field Documentation

§ nTxAck

uint8_t rfc_ieeeRxOutput_s::nTxAck

Total number of transmitted ACK frames.

§ nRxBeacon

uint8_t rfc_ieeeRxOutput_s::nRxBeacon

Number of received beacon frames.

§ nRxData

uint8_t rfc_ieeeRxOutput_s::nRxData

Number of received data frames.

§ nRxAck

uint8_t rfc_ieeeRxOutput_s::nRxAck

Number of received acknowledgement frames.

§ nRxMacCmd

uint8_t rfc_ieeeRxOutput_s::nRxMacCmd

Number of received MAC command frames.

§ nRxReserved

uint8_t rfc_ieeeRxOutput_s::nRxReserved

Number of received frames with reserved frame type.

§ nRxNok

uint8_t rfc_ieeeRxOutput_s::nRxNok

Number of received frames with CRC error.

§ nRxIgnored

uint8_t rfc_ieeeRxOutput_s::nRxIgnored

Number of frames received that are to be ignored.

§ nRxBufFull

uint8_t rfc_ieeeRxOutput_s::nRxBufFull

Number of received frames discarded because the Rx buffer was full.

§ lastRssi

int8_t rfc_ieeeRxOutput_s::lastRssi

RSSI of last received frame.

§ maxRssi

int8_t rfc_ieeeRxOutput_s::maxRssi

Highest RSSI observed in the operation.

§ __dummy0

uint8_t rfc_ieeeRxOutput_s::__dummy0

§ beaconTimeStamp

ratmr_t rfc_ieeeRxOutput_s::beaconTimeStamp

Time stamp of last received beacon frame.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale