Data Fields
SHA2CC26X1_HWAttrs Struct Reference

Hardware-specific configuration attributes. More...

#include <SHA2CC26X1.h>

Data Fields

uint8_t dummy
 

Detailed Description

Hardware-specific configuration attributes.

SHA2CC26X1 hardware attributes are used in the board file by the SHA2_Config struct.

Field Documentation

§ dummy

uint8_t SHA2CC26X1_HWAttrs::dummy

The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale