TI-OpenThread  1.08.06.06
Macros | Typedefs | Functions
LP_CC2674R10_FPGA/thread/cli_mtd/otstack.h File Reference
#include <openthread/config.h>
+ Include dependency graph for LP_CC2674R10_FPGA/thread/cli_mtd/otstack.h:
+ This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define OT_STACK_EVENT_DEV_ROLE_CHANGED   0x06
 
#define OT_STACK_EVENT_NWK_DATA_CHANGED   0x05
 
#define OT_STACK_EVENT_NWK_JOIN_IN_PROGRESS   0x02
 
#define OT_STACK_EVENT_NWK_JOINED   0x03
 
#define OT_STACK_EVENT_NWK_JOINED_FAILURE   0x04
 
#define OT_STACK_EVENT_NWK_NOT_JOINED   0x01
 

Typedefs

typedef void(* OtStack_EventsCallback_t) (uint8_t event, void *aContext)
 

Functions

void handleNetifStateChanged (uint32_t aFlags, void *aContext)
 Callback function registered with the netif. More...
 
void OtStack_joinConfiguredNetwork (void)
 Allows the application to start the network join process via the commissioner using the pre-configured PSKd. More...
 
void OtStack_joinNetwork (const char *pskd)
 Allows the application to start the network join process via the commissioner. More...
 
uint8_t OtStack_joinState (void)
 Returns the current network join event of the OpenThread stack. More...
 
void OtStack_registerCallback (OtStack_EventsCallback_t appCB)
 Allows the application to register callback for ot stack events. More...
 
bool OtStack_setupInterfaceAndNetwork (void)
 Allows the application to attempt to bring up the interface and setup the thread network (thread protocol operation) using the current device dataset. More...
 
bool OtStack_setupNetwork (void)
 Allows the application to setup the thread network(thread protocol operation) after the device has successfully joined the network. More...
 

Macro Definition Documentation

§ OT_STACK_EVENT_NWK_NOT_JOINED

#define OT_STACK_EVENT_NWK_NOT_JOINED   0x01

Events reported to the registered application

§ OT_STACK_EVENT_NWK_JOIN_IN_PROGRESS

#define OT_STACK_EVENT_NWK_JOIN_IN_PROGRESS   0x02

§ OT_STACK_EVENT_NWK_JOINED

#define OT_STACK_EVENT_NWK_JOINED   0x03

§ OT_STACK_EVENT_NWK_JOINED_FAILURE

#define OT_STACK_EVENT_NWK_JOINED_FAILURE   0x04

§ OT_STACK_EVENT_NWK_DATA_CHANGED

#define OT_STACK_EVENT_NWK_DATA_CHANGED   0x05

§ OT_STACK_EVENT_DEV_ROLE_CHANGED

#define OT_STACK_EVENT_DEV_ROLE_CHANGED   0x06

Typedef Documentation

§ OtStack_EventsCallback_t

typedef void(* OtStack_EventsCallback_t) (uint8_t event, void *aContext)

Function Documentation

§ handleNetifStateChanged()

void handleNetifStateChanged ( uint32_t  aFlags,
void *  aContext 
)

Callback function registered with the netif.

Parameters
aFlagsA bit-field indicating specific state that has changed.
aContextA pointer to application-specific context.
Returns
None

§ OtStack_registerCallback()

void OtStack_registerCallback ( OtStack_EventsCallback_t  appCB)

Allows the application to register callback for ot stack events.

Parameters
appCBapplication callback function.
Returns
None

§ OtStack_joinState()

uint8_t OtStack_joinState ( void  )

Returns the current network join event of the OpenThread stack.

Returns
uint8_t event value.

§ OtStack_joinNetwork()

void OtStack_joinNetwork ( const char *  pskd)

Allows the application to start the network join process via the commissioner.

Parameters
pskdPre-shared key of the device.
Returns
None

§ OtStack_joinConfiguredNetwork()

void OtStack_joinConfiguredNetwork ( void  )

Allows the application to start the network join process via the commissioner using the pre-configured PSKd.

Returns
None

§ OtStack_setupNetwork()

bool OtStack_setupNetwork ( void  )

Allows the application to setup the thread network(thread protocol operation) after the device has successfully joined the network.

Returns
bool true if successful in starting the thread protocol operation.

§ OtStack_setupInterfaceAndNetwork()

bool OtStack_setupInterfaceAndNetwork ( void  )

Allows the application to attempt to bring up the interface and setup the thread network (thread protocol operation) using the current device dataset.

Returns
bool true if successful in starting the thread protocol operation.
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale