Z-Stack API Reference  5.40.00.05
_zstack_zdosrcrtgind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t srcAddr
 Source address.
 
uint8_t n_relay
 Number of relay addresses in the list.
 
uint16_t * pRelay
 Array of relay short addresses.
 

Detailed Description

Structure to send a ZDO Source Route Indication.


The documentation for this struct was generated from the following file: