![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.02.05.00
|
Modules | |
| Micro GAP Broadcaster Callbacks | |
| Micro GAP Broadcaster Structures | |
| Micro GAP Constants | |
Files | |
| file | ugap.h |
| Micro BLE GAP API. | |
Functions | |
| bStatus_t | ugap_bcastInit (ugapBcastCBs_t *pCBs) |
| Initialize Micro Broadcaster. More... | |
| bStatus_t | ugap_bcastSetDuty (uint16 dutyOnTime, uint16 dutyOffTime) |
| Set Broadcaster Duty On/Off time. More... | |
| bStatus_t | ugap_bcastStart (uint16 numAdvEvent) |
| Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising. More... | |
| bStatus_t | ugap_bcastStop (void) |
| Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE. More... | |
| bStatus_t ugap_bcastInit | ( | ugapBcastCBs_t * | pCBs | ) |
Initialize Micro Broadcaster.
| pCBs | - a set of application callbacks for Broadcaster |
| bStatus_t ugap_bcastSetDuty | ( | uint16 | dutyOnTime, |
| uint16 | dutyOffTime | ||
| ) |
Set Broadcaster Duty On/Off time.
| dutyOnTime | - Time period during which the Broadcaster is in Advertising state. 100 ms unit. This cannot be 0 unless dutyOffTime is also 0. |
| dutyOffTime | - Time period during which the Broadcaster is in Waiting state. 100 ms unit. If this is 0, Duty Control is disabled regardless of dutyOnTime. |
| bStatus_t ugap_bcastStart | ( | uint16 | numAdvEvent | ) |
Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising.
| numAdvEvent | - # of Advertising events to be performed before the Broadcaster state goes to IDLE. If this is 0, the Broadcaster will keep staying in Advertising or Advertising and Waiting alternately unless an error happens or the application requests to stop. |
| bStatus_t ugap_bcastStop | ( | void | ) |
Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE.