Data Structures | Macros
ECDHCC26X1.h File Reference

Detailed Description

ECDH driver implementation for the CC26X1 family.

============================================================================

This file should only be included in the board file to fill the ECDH_config struct.

Hardware and Implementation Details

Supported Curves

The driver implementation supports the following curves for ECDH:

Curves Supported
NISTP256
Curve25519
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ECDH.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/rom_ecc.h)>
Include dependency graph for ECDHCC26X1.h:

Go to the source code of this file.

Data Structures

struct  ECDHCC26X1_HWAttrs
 ECDHCC26X1 Hardware Attributes. More...
 
struct  ECDHCC26X1_Object
 ECDHCC26X1 Object. More...
 

Macros

#define ECDH26X1_ECC_WINDOW_SIZE   3
 
#define ECDH26X1_ECC_WORKZONE_WORDS   198
 

Macro Definition Documentation

§ ECDH26X1_ECC_WINDOW_SIZE

#define ECDH26X1_ECC_WINDOW_SIZE   3

§ ECDH26X1_ECC_WORKZONE_WORDS

#define ECDH26X1_ECC_WORKZONE_WORDS   198
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale