![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.02.06.00
|
Data Fields | |
| uint8_t | authState |
| TRUE if the pairing was authenticated (MITM) | |
| uint16_t | connectionHandle |
| Connection Handle from controller used to ref the device. | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status | |
| uint8_t | opcode |
| GAP_AUTHENTICATION_COMPLETE_EVENT | |
| smSecurityInfo_t * | pDevSecInfo |
| security information from connected device | |
| smIdentityInfo_t * | pIdentityInfo |
| identity information | |
| smSecurityInfo_t * | pSecurityInfo |
| security information from this device | |
| smSigningInfo_t * | pSigningInfo |
| Signing information. | |
GAP_AUTHENTICATION_COMPLETE_EVENT message format.
This message is sent to the app when the authentication request is complete.
This event will be consumed by the gapbondmgr if it exists.