![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.02.06.00
|
Data Fields | |
| uint16_t | connectionHandle |
| Connection handle of the update. | |
| uint16_t | connInterval |
| Requested connection interval. | |
| uint16_t | connLatency |
| Requested connection latency. | |
| uint16_t | connTimeout |
| Requested connection timeout. | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status | |
| uint8_t | opcode |
| GAP_LINK_PARAM_UPDATE_EVENT | |
| uint8_t | status |
| status from link layer, defined in ll.h | |
GAP_LINK_PARAM_UPDATE_EVENT message format.
This message is sent to the app when the connection parameters update request is complete.