![]() |
![]() |
![]() |
Modules | |
Command Codes | |
Macros | |
#define | ADCBuf_CMD_RESERVED (32) |
#define | ADCBuf_STATUS_RESERVED (-32) |
#define | ADCBuf_STATUS_SUCCESS (0) |
Success status code returned by: ADCBuf_control() More... | |
#define | ADCBuf_STATUS_ERROR (-1) |
Generic error status code returned by ADCBuf_control(). More... | |
#define | ADCBuf_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ADCBuf_control() for undefined command codes. More... | |
#define | ADCBuf_STATUS_UNSUPPORTED (-3) |
An error status code returned if the function is not supported by a particular driver implementation. More... | |
These ADCBuf macros are reservations for ADCBuf.h
#define ADCBuf_CMD_RESERVED (32) |
Common ADCBuf_control command code reservation offset. ADC driver implementations should offset command codes with ADCBuf_CMD_RESERVED growing positively
Example implementation specific command codes:
#define ADCBuf_STATUS_RESERVED (-32) |
Common ADCBuf_control status code reservation offset. ADC driver implementations should offset status codes with ADCBuf_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
#define ADCBuf_STATUS_SUCCESS (0) |
Success status code returned by: ADCBuf_control()
Functions return ADCBuf_STATUS_SUCCESS if the call was executed successfully.
#define ADCBuf_STATUS_ERROR (-1) |
Generic error status code returned by ADCBuf_control().
ADCBuf_control() returns ADCBuf_STATUS_ERROR if the control code was not executed successfully.
#define ADCBuf_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by ADCBuf_control() for undefined command codes.
ADCBuf_control() returns ADCBuf_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
#define ADCBuf_STATUS_UNSUPPORTED (-3) |
An error status code returned if the function is not supported by a particular driver implementation.