![]() |
![]() |
AESCMACCC26XX Hardware Attributes. More...
#include <AESCMACCC26XX.h>
Data Fields | |
uint8_t | intPriority |
Crypto Peripheral's interrupt priority. More... | |
AESCMACCC26XX Hardware Attributes.
AESCMAC26XX hardware attributes should be included in the board file and pointed to by the AESCMAC_config struct.
uint8_t AESCMACCC26XX_HWAttrs::intPriority |
Crypto Peripheral's interrupt priority.
The CC26XX uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).
(7 << 5) will apply the lowest priority.
(1 << 5) will apply the highest priority.
Setting the priority to 0 is not supported by this driver.
HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.