Data Fields
ECCParams_CurveParams Struct Reference

A structure containing the parameters of an elliptic curve. More...

#include <ECCParams.h>

Data Fields

const ECCParams_CurveType curveType
 
const uint8_t * prime
 
const uint8_t * a
 
const uint8_t * b
 
const uint8_t * order
 
const uint8_t cofactor
 
const size_t length
 
const uint8_t * generatorX
 
const uint8_t * generatorY
 

Detailed Description

A structure containing the parameters of an elliptic curve.

Elliptical Curve Cryptography (ECC) prime curve parameters.

Field Documentation

§ curveType

const ECCParams_CurveType ECCParams_CurveParams::curveType

§ prime

const uint8_t* ECCParams_CurveParams::prime

§ a

const uint8_t* ECCParams_CurveParams::a

§ b

const uint8_t* ECCParams_CurveParams::b

§ order

const uint8_t* ECCParams_CurveParams::order

§ cofactor

const uint8_t ECCParams_CurveParams::cofactor

§ length

const size_t ECCParams_CurveParams::length

§ generatorX

const uint8_t* ECCParams_CurveParams::generatorX

§ generatorY

const uint8_t* ECCParams_CurveParams::generatorY

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale