Z-Stack API Reference  6.20.00.04
_zstack_sysnwkinforeadrsp_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t nwkAddr
 Currently assigned short address.
 
zstack_LongAddr_t ieeeAddr
 64 bit IEEE Address
 
zstack_DevState devState
 Current device state.
 
uint16_t panId
 PAN ID.
 
zstack_LongAddr_t extendedPanId
 64 bit extended PAN ID
 
uint16_t parentNwkAddr
 Parent's short address.
 
zstack_LongAddr_t parentExtAddr
 64 bit parent's extended address
 
zstack_deviceTypes_t devTypes
 possible device types
 
uint8_t logicalChannel
 Current network logical channel.
 
zstack_CapabilityInfo_t capInfo
 Capability Flags.
 

Detailed Description

Structure to return the system network information read response.


The documentation for this struct was generated from the following file: