Z-Stack API Reference  6.20.00.04
gpCommissioningNotificationMsg_t Struct Reference

Data Fields

afAddrType_t addr
 APS addressing for ZCL commissioning notification.
 
uint16_t aliasNwk
 Alias for network address.
 
uint8_t seqNum
 Sequence number for ZCL frame.
 
uint8_t len
 Length of buffer to be sent.
 
uint8_t * pbuf
 Pointer to buffer that holds the message.
 

The documentation for this struct was generated from the following file: