TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
attHandleValueInd_t Struct Reference

Handle Value Indication format. More...

Data Fields

uint16 handle
 Handle of the attribute that has been changed (must be first field)
 
uint16 len
 Length of value.
 
uint8 * pValue
 Current value of the attribute (0 to ATT_MTU_SIZE-3)
 

Detailed Description

Handle Value Indication format.

for method ATT_HANDLE_VALUE_IND


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale